This topic describes the updates for the Advanced Real-time Signal Generation capability in software version 2.0, August 2019.
Max number of QZSS satellites is updated to 10, i.e. PRN-193 to PRN-202 are supported, but the QZSS almanac usually contains PRN-193/194/195/199.
Max number of Galileo satellites is updated to 50, i.e. PRN-1 to PRN-50 of Galileo satellites are supported.
The old almanac of year 2014 are removed.
New almanac of year 2019 is included in the installer package:
20190611_GPS.alm, 20190611_BDS.alm, 20190611_GLO.agl, 20190611_GAL.xml, 20190611_QZS.alm
A new scenario file of year 2019 is included in the installer package:
20190611_Beijing.ags
GPS: https://www.navcen.uscg.gov/?pageName=gpsAlmanacs
Beidou: http://www.csno-tarc.cn/support/downloads or https://www.glonass-iac.ru/en/BEIDOU/
Glonass: ftp://ftp.glonass-iac.ru/MCC/ALMANAC/
Galileo: https://www.gsc-europa.eu/system-status/almanac-data